4.2.2 qmm_queue_append Function
C
qmm_status_t qmm_queue_append(queue_t *q, buffer_t *buf)Summary
Appends a buffer into the queue
Description
This function appends a buffer into the designated queue
Precondition
qmm_queue_init should have called for initilazing the particular queue before using it
Parameters
| Param | Description |
|---|---|
| q | Queue into which buffer should be appended |
| buf | Pointer to the buffer that should be appended into the queue. Note that this pointer should be same as the pointer returned by bmm_buffer_alloc |
Returns
QUEUE_SUCCESS - Buffer gets appended successfully QUEUE_FULL - Designated queue is full
Example
queue_t app_queue; buffer_t *app_buf; // Allocate the buffer app_buf = bmm_buffer_alloc(LARGE_BUFFER_SIZE); uint8_t queue_size = 10; qmm_queue_init(&app_queue, queue_size); // Append buffer in queue qmm_queue_append(&app_queue, app_buf);
Remarks
None