4.2.4 qmm_queue_remove Function
C
buffer_t* qmm_queue_remove(queue_t *q, search_t *search)
Summary
Removes a buffer from queue.
Description
This function removes a buffer from queue
Precondition
qmm_queue_init should have called for initilazing the particular queue before using it and buffer should be appended before removing it
Parameters
| Param | Description |
|---|---|
| q | Queue from which buffer should be removed |
| search | Search criteria. If this parameter is NULL, first buffer in the queue will be removed. Otherwise buffer matching the criteria will be removed |
Returns
return - Pointer to the buffer header, if the buffer is successfully removed, NULL otherwise.
Example
queue_t app_queue; buffer_t *app_buf; // Allocate the buffer app_buf = bmm_buffer_alloc(LARGE_BUFFER_SIZE); uint8_t queue_size = 10; qmm_queue_init(&app_queue, queue_size); // Append buffer in queue qmm_queue_append(&app_queue, app_buf); //Remove buffer from queue app_buf = qmm_queue_remove(&app_queue, NULL);
Remarks
None