3 Installing MCHPRT3 Tool
This section provides step-by-step instructions for installing the MCHPRT3 tool on a Windows operating system. The following are the steps to complete the installation:
-
Extract the
MCHPRT3_Setup_v1.0.2.8091.zip.Figure 3-1. MCHPRT3 Setup File Note: The version number provided here is for reference. For the most up-to-date version, refer to the MCHPRT3 page. -
Execute the
MCHPRT3_Setup.exe. The following screen appears:- Click Next to continue the installation procedure.
Figure 3-2. MCHPRT3 Setup Welcome Screen -
Check “I accept the terms of the License Agreement”.
- Click Next to continue.
Figure 3-3. License Agreement Screen -
Click Browse to change the destination folder to the desired location, then click Install to continue the installation procedure.
- By default, the MCHPRT3 tool installs the package in the C:\Microchip\ folder.
Figure 3-4. Destination Folder Selection Screen -
If the system does not have the “Microsoft Visual C++ Redistributable for Visual Studio 2015, 2017, and 2019” installed, the following screen appears.
- Click OK to install it.
Figure 3-5. Microsoft Visual C++ Redistributable Installation Prompt -
Check “I accept the license terms and conditions” and click Install to continue.
Figure 3-6. Microsoft Visual C++ Redistributable License Agreement Screen -
Click Close to continue.
Figure 3-7. Microsoft Visual C++ Redistributable Installation Complete Screen Note:If an error occurs when installing the Microsoft Visual C++ 2017 Redistributable (x86) – 14.16.27052, click the log file link as shown below.Figure 3-8. Microsoft Visual C++ Setup Failed If the last line in the log file content is “Error 0x80070666: Cannot install a product when a newer version is installed,” it means that your system may already have a higher version installed. Therefore, it is fine to use the tool.
-
Check “Open the installed directory” and click Finish to continue.
Figure 3-9. Installation Complete Screen -
The file browser opens with the install directory.
Figure 3-10. Installed Directory in File Browser