7 WILCS02_WINCS02 Python 3 Information
This chapter describes the Python 3 example information of the WILCS02_WINCS02. For more details, refer to the
Python3_Example.chm.
Refer to the example code in the WILCS02_WINCS02 package
example folder, which provides details on how to use the WILCS02_WINCS02.dll file with the Python
language to control the WILCS02_WINCS02.