Running the demo involves verifying the imaging and video settings using the Video Control GUI,
and then observing the video output on the HDMI monitor.
To use the demo GUI, perform the following steps:
Start the Video Control GUI from the installation directory, see the following figure.Figure 6-1. Video Control GUI
In the I/O list, click the
second largest COM port, and then click
Connect.Figure 6-2. Connecting the GUI and Video KitThe following figure shows that the Connect
button turns green indicating a successful
connection.Figure 6-3. Connection Successful
Move the corresponding sliders appropriately to adjust the contrast and brightness and observe the change on the HDMI monitor.Figure 6-4. Adjusting Contrast and Brightness
Similarly, move the sliders to adjust the color balance of the image using the color balance sliders.Figure 6-5. Color Balance
Important:PIP Menu, Panning, Histogram, and Edge Detection options are not supported in this demo.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.