4.4.2 Sleep Sequence
Upon completion of the use of the TA010-TFLXAUTH
by the system, it is recommended that the system issue a sleep sequence to put the
device into Low-Power mode. This sequence consists of the proper device address followed
by the value of 0x01
as the word address followed by a Stop condition.
This transition to the Low-Power state causes a complete reset of the device’s internal
command engine and input/output buffer. It can be sent to the device at any time when it
is awake and not busy.