2 Implementation
The example code is written for "Atmel START". It can be downloaded from the "BROWSE EXAMPLES" entry of Atmel START for both Atmel Studio 7 and IAR IDE.
Project Name: AVR136 Software PWM (view User Guide for detailed requirements).
Double-click the downloaded .atzip file and the project will be imported to Atmel Studio 7.
To import the project in IAR, refer "Atmel START in IAR" , select ‘Atmel Start Output in External Tools → IAR'.