6.4.5 Delete Configuration File
Use this command to delete any of the writable configuration files stored in flash, including startup-config.
Command Syntax:
delete <path>|
Argument |
Description | |
|
Parameter |
| File in FLASH. Syntax: <flash:filename>. A valid file name
is a text string drawn from the alphabet (A–Za–z), digits (0–9), dot (.), hyphen (-),
and underscore (_). The maximum length is 63 characters, and the hyphen must not be
the first character. The file name content that contains only ‘.’ is not
allowed. |
|
Default |
N.A | |
|
Mode |
EXEC | |
|
Usage |
Use this command to delete unit configuration stored in flash | |
|
Example | Example
1: | |