3.4 Setting up the AGX Orin Developer Kit
To set up the AGX Orin developer kit, perform the following steps:
- Run the steps in the Getting Started with Jetson AGX Orin Developer Kit.
- While on the getting started page, choose the “Default setup flow” instead of the “Optional Setup Flow” and when scrolling down, choose “Initial setup with display attached” instead of the “Initial setup in a headless configuration”.Note: This step can take a long time. Make sure you have a stable internet connection.