3.3 Camera Setup
To set up the camera, perform the following steps:
- Make sure the MPF200-ETH-SENSOR-BRIDGE board is powered OFF.
- Connect the IMX477 Camera module to
J14 MIPI connector using the 22-pin to 22-pin camera cable, as shown in the
following figure.
Figure 3-2. Connecting the Image Sensor to the MIPI CSI-2 Port of the Sensor Bridge - Insert SFP+ to RJ45 converter into the SFP cage on J5.
- Connect the Ethernet cable from the
SFP+ RJ45 port to the Ethernet port on NVIDIA Jetson AGX Orin Developer Kit, as
shown in the following figure.
Figure 3-3. Jetson AGX Orin Developer Kit Callout - Connect the 12V power adapter to the J25 power input port.
- To turn on the board, slide the switch SW1 to the ON position.