1.6 Result Presentation
The ADC can be configured to present conversion results in the following formats:
- 12 bits, right adjusted
- 8 bits, right adjusted
- 12 bits, left adjusted
The ADC resolution is configured using the Conversion result Resolution bit field (RESOLUTION) in Control Register B (CTRLB).
The result will be stored in the result registers for each channel. The channels have separate flags to indicate when a new conversion is ready. If the result is not read before a new conversion is done, the current result will be lost.
The DMA can be set up to transfer the result from the result register into the SRAM when a new conversion is ready. This can be done for all channels when doing sweep and store all channels in one burst.