4.1.1 ATSAMR30M Sensor Board and mikroBUS Click Board Interface
The receptacles (J1 and J2) provide the interface to use the ATSAMR30M Sensor Board with a Click Board. The connection of the sensor board with an FTDI Click Board is shown in the following figure. Similarly, the sensor board can also be connected with a Click Board that has different functionality to demonstrate applications based on customer requirements.
The ATSAMR30M sensor board interfaced with the FTDI Click Board could be used as an alternate to the setup shown in Figure 4-1. The FTDI Click Board could power the ATSAMR30M sensor board and act as the UART-USB Converter. This setup can only be operated at 3.3V as the FTDI Click Board is the power source.