The timer can be configured to be used as a hardware-based switch debouncer
as per the settings shown in Table 2-10.
Table 2-10. Timer Configuration
Timer Setting
Value
START
Either ERS Edge
RESET
At Start + PR Match
STOP
PR Match
CSYNC (Clock Sync)
Sync
EPOL (ERS Polarity)
True Level (to trigger to rising edge)
Inverted Level (to trigger to falling edge)
PR (Period Register)
Desired minimum pulse width
Initialize the timer counter by setting the CLR command. When the input rises
(changes from 0 to 1), the counter will begin counting. Any more input changes will be
ignored unless a rising edge occurs near the PR match, which will override the Stop
condition, reset the counter, and continue counting. This is shown in Figure 2-13.
With any input change, the counter is reset and begins counting. When the
counter reaches PR, the output changes and causes an interrupt. This is shown in Figure 2-13 below. The
interrupt software, knowing that the input is stable, can read the raw switch input to
determine if the switch is open or closed. Alternatively, the D flip-flop in a CLC may
be used to sample the input, as illustrated below in Figure 2-14.Figure 2-13. Switch DebouncerFigure 2-14. UTMR and CLC
Connection