1.5 Cyclic Redundancy Check
Cyclic Redundancy Check (CRC) is used by 1-Wire devices to ensure data integrity. The theory behind CRC is outside the scope of this document and will not be further discussed. See “Reference, 2” for more information on CRC.
Two different CRC’s are commonly found in 1-Wire devices. One 8-bit CRC (Dallas One Wire CRC, DOW-CRC, or simply CRC8) and one 16-bit CRC (CRC16). CRC8 is used in the ROM section of all devices. CRC8 is also, in some devices, used to verify other data like commands issued on the bus. CRC16 is used by some devices to check for errors on larger data sets.
The hardware equivalent of the 8-bit CRC used on the 64-bit identifier is
shown in the first figure below. The blocks represent the individual bits in an 8-bit
shift register. The equivalent CRC polynomial is
X8+X5+X4+1.
The hardware equivalent of the 16-bit CRC used in some 1-Wire devices is
shown in the figure below. The blocks represent the individual bits in a 16-bit shift
register. The equivalent polynomial is
X16+X15+X2+1.