7.1.1 PID Controller Background
A PID controller responds to an error signal in a closed control loop and attempts to adjust the controlled quantity in order to achieve the desired system response. The controlled parameter can be any measurable system quantity, such as speed, voltage or current. The output of the PID controller can control one or more system parameters that will affect the controlled system quantity. For example, a speed control loop in a Sensorless Brushless DC motor application can control the PWM duty cycle directly, or it can set the current demand for an inner control loop that regulates the motor currents. The benefit of the PID controller is that it can be adjusted empirically by adjusting one or more gain values and observing the change in system response.
A digital PID controller is executed at a periodic sampling interval, and it is assumed that the controller is executed frequently enough so that the system can be properly controlled. For example, the current controller in the Sensorless Brushless DC motor application is executed in every PWM cycle, since the motor can change very rapidly. The speed controller in such an application is executed at the medium event rate (100 Hz) because motor speed changes will occur relatively slowly due to mechanical time constants.
The error signal is formed by subtracting the desired setting of the parameter to be controlled from the actual measured value of that parameter. This sign of the error indicates the direction of change required by the control input.
The Proportional (P) term of the controller is formed by multiplying the error signal by a P gain. This will cause the PID controller to produce a control response that is a function of the error magnitude. As the error signal becomes larger, the P term of the controller becomes larger to provide more correction.
The effect of the P term will tend to reduce the overall error as time elapses. However, the effect of the P term will reduce as the error approaches zero. In most systems, the error of the controlled parameter will get very close to zero but will not converge. The result is a small remaining steady state error. The Integral (I) term of the controller is used to fix small steady state errors. The I term takes a continuous running total of the error signal. Therefore, a small steady state error will accumulate into a large error value over time. This accumulated error signal is multiplied by an I gain factor and becomes the I output term of the PID controller.
The Differential (D) term of the PID controller is used to enhance the speed of the controller and responds to the rate of change of the error signal. The D term input is calculated by subtracting the present error value from a prior value. This delta error value is multiplied by a D gain factor that becomes the D output term of the PID controller. The D term of the controller produces more control output the faster the system error is changing.
It should be noted that not all PID controllers will implement the D or, less commonly, the I terms. For example, the speed controller in a Brushless DC motor application described in Microchip Application Note AN901 does not have a D term due to the relatively slow response time of motor speed changes. In this case, the D term could cause excessive changes in PWM duty cycle that could affect the operation of the sensorless algorithm and produce overcurrent trips.