9.9.1 __external__ Type Qualifier
This qualifier is used to indicate that the compiler should access variables or pointer targets which have been located in external memory. See the External Memory Access section for more information on how the memory space is configured and access routines are defined.
The qualifier is used as in the following example.
__external__ int external_array[256]
__attribute__((space(external(external_memory))));
__external__ char * myExternalPointer;
In addition to the qualifier, the array uses a memory space which would
need to be predefined. The pointer in this example does not use the space
attribute as it is located in data memory, but the qualifier indicates how the pointer
targets are to be accessed. For more information on the space attribute,
see the Variable Attributes section. For
basic information on the memory layout and how program memory is accessed by the device,
see the Address Spaces section.
For more on the qualifier, see the External Memory Access section.