5.6.4 xc32-ld (32-bit MCU Linker)
A subset of command-line options may be specified in MPLAB X IDE. Select a category and then set up linker options. For additional options, see the “MPLAB® XC32 Assembler, Linker and Utilities User’s Guide for PIC32A MCU” (DS-50003839). See also “Options Page Features.”
| Option | Description | Command Line |
|---|---|---|
| Heap size | Specify the size of the heap in bytes. Allocate a run-time heap of size bytes for use by C programs. The heap is allocated from unused data memory. If not enough memory is available, an error is reported. | --heap size |
| Min stack size | Specify the minimum size of the stack in
bytes. By default, the linker allocates all unused data memory for the run-time
stack. Alternatively, the programmer may allocate the stack by declaring two
global symbols: __SP_init and __SPLIM_init.
Use this option to ensure that at least a minimum sized stack is available. The
actual stack size is reported in the link map output file. If the minimum size
is not available, an error is reported. | --stack size |
| Allow overlapped sections | Check to not check section addresses for overlaps. Uncheck to check for overlaps. | --check-sections
|
| Init data sections | Check to support initialized data. Uncheck to not support. | --data-init
|
| Create default ISR | Check to create an interrupt function for unused
vectors. Uncheck to not create a default ISR. | --isr
|
| Remove unused sections | Check to not enable garbage collection of unused input sections (on some targets). Uncheck to enable garbage collection. | --no-gc-sections
|
| Stack guardband size | Enter a stack guardband size to ensure that enough stack space is available to process a stack overflow exception. | --stackguard=size |
| Additional driver options | Type here any additional driver options not existing in this GUI otherwise. The string you introduce here will be emitted as is in the driver invocation command. | |
| Use response file to link | Check to create a makefile that uses a
response file for the link step. In Windows® OS, you have
a maximum command line length of 8191 chars. When linking long programs, the
link line might go over this limit. MPLAB XC32
provides a response file work-around. See MPLAB X IDE
documentation, Troubleshooting section, for details. Uncheck to not use a response file. |
| Option | Description | Command Line |
|---|---|---|
| Linker symbols | Create a global symbol in the output file
containing the absolute address (expr). You may use this
option as many times as necessary to define multiple symbols in the command
line. A limited form of arithmetic is supported for the expr
in this context: you may give a hexadecimal constant or the name of an existing
symbol, or use + and - to add or subtract hexadecimal constants or
symbols. | --defsym=sym |
| Define Linker macros | Add linker macros. | -Dmacro |
| Symbols | Specify symbol information in the output. | |
| - Keep all | ||
| - Strip debugging info | --strip-debug (-S) | |
| - Strip all symbol info | --strip-all (-s) |
| Option | Description | Command Line |
|---|---|---|
| Which areas to fill | Specify which area of Flash memory to fill. No Fill - None (default). Fill All Unused - Fill all unused memory. Provide Range to fill - Fill a range of memory. Enter a range under “Memory Address Range.” | |
| How to fill it | Specify how to fill Flash memory. Provide sequence of values - Provide a sequence under the Sequence option. Constant or incrementing value - Provide either:
| |
| Sequence | When Provide sequence of values is
selected, enter a sequence. The form is n1, n2, ...
where n1 uses C syntax. Example: 0x10, 25, 0x3F, 16. | --fill=sequence |
| Constant | When Constant or incrementing value is
selected, enter a constant. Specify the constant using C syntax (e.g.,
0x for hex, 0 for octal).
Example: 0x10 is the same as 020 or 16. | --fill=constant |
| Increment/Decrement | When Constant or incrementing value is
selected, you may select to increment or decrement the initial value of
“Constant” on each consecutive address. No Incrementing - Do not change constant value. Increment Const - Increment the constant value by the amount specified under the option “Increment/Decrement Constant.” Decrement Const - Decrement the constant value by the amount specified under the option “Increment/Decrement Constant.” | |
| Increment/Decrement Constant | When Increment Const or Decrement
Const is selected, enter a constant increment or decrement value.
Specify the constant using C syntax (e.g., 0x for hex,
0 for octal). Example: 0x10 is the same as 020 or 16. | --fill=constant+=incr
|
| Memory Address Range | When Provide Range to fill is
selected, enter the range here. Specify range as Start:End where Start and End
use C syntax. Example 0x100:0x1FF is the same as 256:511 . | --fill=value@range |
| Option | Description | Command Line |
|---|---|---|
| Libraries | Add libraries to be linked with the project files. You may add more than one. | --library=name |
| Library directory | Add a library directory to the library search path. You may add more than one. | --library-path=“name” |
| Force linking of objects that might not be compatible | Check to force linking of objects that might
not be compatible. The linker will compare the project device to information
contained in the objects combined during the link. If a possible conflict is
detected, an error (in the case of a possible instruction set incompatibility)
or a warning (in the case of possible register incompatibility) will be
reported. Specify this option to override such errors or warnings. Uncheck to not force linking. | --force-link
|
| Don’t merge I/O library functions | Check to not merge I/O library functions. Do
not attempt to conserve memory by merging I/O library function calls. In some
instances the use of this option will increase memory usage. Uncheck to merge I/O library functions to conserve memory. | --no-smart-io
|
| Exclude standard libraries | Check to not use the standard system startup
files or libraries when linking. Only use library directories specified on the
command line. Uncheck to use the standard system startup files and libraries. | --nostdlib |
| Option | Description | Command Line |
|---|---|---|
| Generate map file | Create a map file. | -Map=“file” |
| Display memory usage | Check to print memory usage report. Uncheck to not print a report. | --report-mem |
| Generate cross-reference file | Check to create a cross-reference table. Uncheck to not create this table. | --cref |
| Warn on section realignment | Check to warn if start of section changes due
to alignment. Uncheck to not warn. | --warn-section-align |
| Trace Symbols | Add/remove trace symbols. | --trace-symbol=symbol |