5.6 Project Setup

To set up an MPLAB X IDE project for the first time, use the built-in Project Wizard (File > New Project). In this wizard, you will be able to select a language toolsuite that uses the XC32 language tools. For more on the wizard and MPLAB X IDE projects, see MPLAB X IDE documentation.

Once you have a project set up, you may then set up properties of the tools in MPLAB X IDE (see figure below).

  1. From the MPLAB X IDE menu bar, select File > Project Properties to open a window to set/check project build options.
  2. Under Conf:[default], select a tool from the tool collection to set up.
    Figure 5-3. Project Properties Window