11.9.2 Near or Far Code
Functions that are near may call each other more efficiently than those
which are not. If it is known that all functions in an application are near, then the
default -msmall-code command line option can be used when compiling
each module to direct the compiler to use a more efficient form of the function
call.
If this default option is not suitable, a linker error message will reported and the following alternatives are available:
- It is possible to compile some modules of an application using the
-msmall-codecommand line option. In this case, only function calls in those modules will use a more efficient form of the function call. - If the
-msmall-codecommand-line option has been used, then the compiler may be directed to use the long form of the function call for an individual function by tagging it with thefarattribute. - Instead of using command-line options, which have module scope, the
compiler may be directed to call individual functions using the near (small) or far
(large) code models by tagging their declarations with the
nearorfarattribute. - Group locally referent code together by using named sections or keep this code in common translation units.
The linker will produce an error message if the function declared to be near cannot be reached by one of its callers using a more efficient form of the function call.