1.5.4.4.4 SRV_TIME_MANAGEMENT_CountToUS Function
C
uint32_t SRV_TIME_MANAGEMENT_CountToUS(uint64_t counter);
Summary
Converts a given time in cycles and returns the equivalent value in microseconds.
Description
This routine makes use of SYS_TIME service to convert a value in cycles and return a value in microseconds.
Precondition
SYS_TIME_Initialize routine must have been called before.
Parameters
| Param | Description |
|---|---|
| counter |
Cycles of the counter |
Returns
Converted time in microseconds.
Example
uint64_t timeReceptionCounter;
uint32_t timeUs;
timeUs = SRV_TIME_MANAGEMENT_CountToUS(timeReceptionCounter);
printf("Transmission Reception time:%u", timeUs);
Remarks
Cycles to convert should be as close as possible to the current value to avoid an overflow.