1.5.4.4.3 SRV_TIME_MANAGEMENT_USTCount Function
C
uint64_t SRV_TIME_MANAGEMENT_USToCount(uint32_t timeUs);
Summary
Converts a given time to microseconds and returns the equivalent value in cycles.
Description
This routine makes use of SYS_TIME service to convert a value in microseconds and return a value in cycles.
Precondition
SYS_TIME_Initialize routine must have been called before.
Parameters
| Param | Description |
|---|---|
| timeUS |
Time in microseconds |
Returns
Value of cycles counter.
Example
uint64_t nextTimeCounter;
uint32_t nextTimeUS;
uint32_t currentTimeUS;
currentTimeUS= SRV_TIME_MANAGEMENT_GetTimeUS();
nextTimeUS = currentTimeUS + 1000;
nextTimeCounter = SRV_TIME_MANAGEMENT_USToCount(nextTimeUS);
Remarks
Time to convert should be as close as possible to the current time to avoid an overflow.