1.5.4.4.6 SRV_TIME_MANAGEMENT_CbRegisterMS Function
C
SYS_TIME_HANDLE SRV_TIME_MANAGEMENT_CbRegisterMS ( SYS_TIME_CALLBACK callback,
uintptr_t context, uint32_t ms, SYS_TIME_CALLBACK_TYPE type );
Summary
Registers a function with the time system service to be called back when the requested number of miliseconds have expired (either once or repeatedly).
Description
This routine registers a function in SYS_TIME to be called back when the requested delay (specified in miliseconds) has completed. The caller must identify if the timer should call the function once or repeatedly every time the given delay period expires.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| callback |
Pointer to the function to be called. |
| context | A client-defined value that is passed to the callback function. |
| ms | Time period in miliseconds. |
| type |
Type of callback requested. If type is SYS_TIME_SINGLE, the callback function will be called once when the time period expires. If type is SYS_TIME_PERIODIC, the callback function will be called repeatedly, every time the time period expires until the timer object is stopped or deleted. |
Returns
SYS_TIME_HANDLE - A valid timer object handle if the call succeeds.
SYS_TIME_HANDLE_INVALID if it fails.
Example
void MyCallback ( uintptr_t context);
SYS_TIME_HANDLE handle = SRV_TIME_MANAGEMENT_CbRegisterMS(MyCallback, (uintptr_t)0, 1000, SYS_TIME_PERIODIC);
if (handle != SYS_TIME_HANDLE_INVALID)
{
}
Remarks
This service will give a callback after the requested number of microseconds or longer have elapsed, depending on system performance. In tick-based mode, the requested delay will be ceiled to the next timer tick. For example, if the timer tick is set to 1 msec and the requested delay is 1500 usec, a delay of 2 msec will be generated.
Delay values of 0 will return SYS_TIME_ERROR.