Reading the AT25512 via the SO pin requires the
following sequence. After the CS line is pulled low to select a
device, the READ (03h) instruction is transmitted via the SI line
followed by the 16‑bit address to be read. Refer to Table 7-1 for the address bits for AT25512.
Table 7-1. AT25512 Address Bits
Address
AT25512
AN
A15—A0
Upon completion of the 16‑bit address,
any data on the SI line will be ignored. The data (D7‑D0) at the specified address is
then shifted out onto the SO line. If only one byte is to be read, the
CS line should be driven high after the data comes out. The
read sequence can be continued since the byte address is automatically incremented and
data will continue to be shifted out. When the highest‑order address bit is reached, the
address counter will rollover to the lowest‑order address bit allowing the entire memory
to be read in one continuous read cycle regardless of the starting address.Figure 7-1. Read Waveform
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.