4.3.2.4 Data Input Bit Frame
A data input bit frame can be used by the host to transmit either a logic ‘0’ or a logic ‘1’ data bit to the ECC204-TFLXAUTH. The input bit frame is initiated when the host drives the SI/O line low. The length of time that the SI/O line is held low will dictate whether the host is transmitting a logic ‘0’ or a logic ‘1’ for that bit frame. For a logic ‘0’ input, the length of time that the SI/O line must be held low is defined as tLOW0. Similarly, for a logic ‘1’ input, the length of time that the SI/O line must be held low is defined as tLOW1.
The ECC204-TFLXAUTH will sample the state of the SI/O line
after the maximum tLOW1 but prior to the minimum tLOW0 after SI/O is driven below the VIL threshold to determine if the data input is a logic ‘0’
or a logic ‘1’. If the host is still driving the line low at the sample
time, the ECC204-TFLXAUTH will decode that bit frame as a logic
‘0’ as SI/O will be at a voltage less than VIL. If the host has already released the SI/O line, the ECC204-TFLXAUTH sees a voltage level greater than or equal to
VIH because of the external pull-up resistor, and that
bit frame is decoded as a logic ‘1’.
A logic ‘0’ condition has multiple uses similar to I2C sequences. It is used to signify a ‘0’
data bit and it is also used for an ACK response. Additionally, a logic
‘1’ condition is used for a NACK response in addition to the
nominal ‘1’ data bit.
The figures below depict the logic ‘0’ and logic ‘1’ input bit frames.
0’ Input Condition Waveform1’ Input Condition Waveform