2.3 Erasing External Antenna Cal
To erase the External Antenna Cal effect, use the following command:
iconfig --erasePostCalParameters:
- None
Return Value:
“done”: Upon successful execution of the command, this return value is provided.
Example:
iconfig --erasePostCal