4 MPLAB® X MCC
MPLAB® X MCC comes with a driver for the OPAMP module allowing for easy configuration of the module. The MCC module comes with nine predefined configurations as well as a custom mode.
| Op Amp Combinations | Posible Configurations |
|---|---|
| OP1-OP2 | Differential Amplifier, Cascaded (Two) Non-Inverting PGA, Cascading (Two) Inverting PGA |
| OP2-OP1 | Differential Amplifier, Cascaded (Two) Non-Inverting PGA, Cascading (Tow) Inverting PGA |
| OP2-OP0 | Differential Amplifier, Cascading (Two) Inverting PGA |
| OP0-OP1-OP2 | Instrumentation Amplifier, Cascaded (Three) Non-Inverting PGA, Cascaded (Three) Inverting PGA |
| OP1-OP2-OP0 | Instrumentation Amplifier, Cascaded (Three) Inverting PGA |
| OP2-OP0-OP1 | Instrumentation Amplifier, Cascaded (Three) Inverting PGA |
If the Single OPAMPs option is selected, each op amp can be enabled and configured separately, as seen in Figure 1. If the Dual and Single OPAMPs or Triple OPAMPs option is selected, the configuration of the dual or triple configuration can be selected. The configuration of the single op amp, if any, and how the op amps should be connected, is shown in Figure 2.
After selecting the global options and hardware settings, there is one banner for each enabled op amp where the op amp specific options can be selected. For each configuration, there is an accompanying picture to show how the configuration looks. The “OP0 Hardware Settings” will have different fields grayed out depending on the configurations. The grayed-out field cannot be changed as that would break the configuration, but they are visible to show how the op amp is configured. The other field can be changed as normal and typically change the input or the gain of the configuration.
The last options are under “OPn Advanced Hardware” Settings. By default, they are configured as always on and in normal output mode. This way, the op amp works as soon as it is initialized. The settle time is set to the maximum, as this is the recommended value for an unknown load.