5.8.5.4 XC-DSC Linker - Libraries
| Option | Description | Command Line |
|---|---|---|
| Libraries | Add libraries to be linked with the project files. You may add more than one. | --library=name |
| Library directory | Add a library directory to the library search path. You may add more than one. | --library-path=“name” |
| Force linking of objects that might not be compatible | Check to force linking of objects that
might not be compatible. The linker will compare the project device to
information contained in the objects combined during the link. If a
possible conflict is detected, an error (in the case of a possible
instruction set incompatibility) or a warning (in the case of possible
register incompatibility) will be reported. Specify this option to
override such errors or warnings. Uncheck to not force linking. | --force-link
|
| Don’t merge I/O library functions | Check to not merge I/O library
functions. Do not attempt to conserve memory by merging I/O library
function calls. In some instances the use of this option will increase
memory usage. Uncheck to merge I/O library functions to conserve memory. | --no-smart-io
|
| Exclude standard libraries | Check to not use the standard system
startup files or libraries when linking. Only use library directories
specified on the command line. Uncheck to use the standard system startup files and libraries. | --nostdlib |