5.8.3.4 XC-DSC C Compiler - Preprocessing and Messages

Table 5-24. Preprocessing and Messages Options
OptionDescriptionCommand Line
C include dirs

Add dir to the main include path.

Relative paths are from the project directory.

If you want a single place to have include paths for compiler and assembler, use the include paths in the global options node.

For more information, see 5.7.8 Additional Search Paths and Directories.

-I"dir"
Define C macrosDefine macro macro with the string 1 as its definition.-Dmacro
ANSI-std C supportCheck to support all (and only) ANSI C programs.

Uncheck to support ANSI and non-ANSI programs.

-ansi
Use CCI syntaxCheck if your code is written per the Common C Interface (CCI) syntax (see 25 Common C Interface).

Uncheck if you are not.

-mcci
Use IAR syntaxCheck if your code is written per the Embedded Compiler Compatibility Mode syntax for IAR (see 24 Embedded Compiler Compatibility Mode).

Uncheck if you are not.

-mext=IAR
ErrataThis option enables specific errata work-arounds identified by ID.

Valid values for ID change from time to time and may not be required for a particular variant. The ID all will enable all currently supported errata work-arounds. The ID list will display the currently supported errata identifiers along with a brief description of the errata.

-merrata=id
Smart IO forwarding levelThis option attempts to statically analyze format strings passed to printf, scanf and the ‘f’ and ‘v’ variations of these functions. Uses of nonfloating point format arguments will be converted to use an integer-only variation of the library functions. Equivalent to-msmart-io=n option where n equals:
  • 0 - disables this option.
  • 1 - only convert the literal values it can prove.
  • 2 - causes the compiler to be optimistic and convert function calls with variable or unknown format arguments.
-msmart-io=n
Smart IO format stringSpecifies what the format arguments are when the compiler is unable to determine them.
Make warnings into errorsCheck to halt compilation based on warnings as well as errors.

Uncheck to halt compilation based on errors only.

-Werror
Additional warningsCheck to enable all warnings.

Uncheck to disable warnings.

-Wall
Enable cast alignWarn whenever a pointer is cast such that the required alignment of the target is increased. For example, warn if a char * is cast to an int * on machines where integers can only be accessed at two- or four-byte boundaries.-Wcast-align
Strict ANSI warnings

Check to issue all the warnings demanded by strict ISO C and ISO C++; reject all programs that use forbidden extensions and some other programs that do not follow ISO C and ISO C++.

Uncheck to issue all warnings.

-pedantic
Disable ISR warnDisable warning for inappropriate use of ISR function names. By default the compiler will produce a warning if the interrupt is not attached to a recognized interrupt vector name. This option will disable that feature.-mno-isr-warn
Enable SFR warningsEnable warnings related to SFRs.-msfr-warn=on|off
Enable macro expansion in pragma config valueThis option will enable the support for macro expansion in #pragma config value. For example:
#define BAR 0x1234
#pragma config FOO=BAR
After preprocessing the file the #pragma config will become:
#pragma config FOO=0x1234 
-mexpand-pragma-config