23.9 Setup for PWM Operation Using PWMx Output Pins
Take these steps when configuring the module for PWM operation using the PWMx pins:
- Disable the PWMx pin output driver(s) by setting the associated TRIS bit(s).
 - Clear the PWMxCON register.
 - Load the T2PR register with the PWM period value.
 - Load the PWMxDCH register and bits [7:6] of the PWMxDCL register with the PWM duty cycle value.
 - Configure and start Timer2:
- Clear the TMR2IF interrupt flag bit of the PIR4 register(1)
 - Select the timer clock source to be FOSC/4 using the TxCLKCON register. This is required for correct operation of the PWM module.
 - Configure the T2CKPS bits of the T2CON register with the Timer2 prescale value
 - Enable Timer2 by setting the T2ON bit of the T2CON register
 
 - Enable the PWM output pin and wait until Timer2 overflows, the TMR2IF bit of the PIR4 register is set.(2)
 - Enable the PWMx pin output driver(s) by clearing the associated TRIS bit(s) and setting the desired pin PPS control bits.
 - Configure the PWM module by loading the PWMxCON register with the appropriate values.
 
Note: 
   - To send a complete duty cycle and period on the first PWM output, the above steps must be followed in the order given. If it is not critical to start with a complete PWM signal, then move step 8 to replace step 4.
 - For operation with other peripherals only, disable the PWMx pin outputs.