4.2.1.4 APS_BindReq_t Struct
C
typedef struct
{
/** Endian "[LE]" The source IEEE address for the binding entry. */
ExtAddr_t srcAddr;
/** The source endpoint for the binding entry. Valid range: 0x01-0xFE. */
Endpoint_t srcEndpoint;
/** Endian "[LE]" The identifier of the cluster on the source device
* that is to be bound to the destination device. */
ClusterId_t clusterId;
/** The addressing mode for the destination address. This parameter can take
* a value from the following list:
APS_GROUP_ADDRESS - 16-bit dst.group is used to identify the destination group
APS_EXT_ADDRESS - the destination node is identified with extended address;
* dst.unicast.extAddr holds the extended address, dst.unicast.endpoint holds the endpoint
**/
APS_AddrMode_t dstAddrMode;
/** Endian "[LE]" The destination address for the binding entry. */
APS_DstBindAddr_t dst;
/** The field to keep the result of the request*/
APS_BindConf_t confirm;
} APS_BindReq_t;
Description
struct APS_BindReq_t apsmeBind.h "aps.h" The structure used to hold parameters for APS_BindReq() A pointer to an instance of this type should be passed to APS_BindReq() function. The structure conforms to the APSME-BIND.request primitive defined in ZigBee specification.