4.2.1.13 APS_Status_t Enum
C
typedef enum
{
/** A request has been executed successfully. */
APS_SUCCESS_STATUS = 0x00,
/** IEEE 802.15.4-2006, Table 83. */
/** Valid values of the Association Status field. */
APS_MAC_PAN_AT_CAPACITY_STATUS = 0x01,
APS_MAC_PAN_ACCESS_DENIED_STATUS = 0x02,
/** The supplied endpoint was equal to 0x00 or 0xff. */
APS_INVALID_EP_STATUS = 0x82,
/** A transmit request has failed since the ASDU is too large and fragmentation
* is not supported. */
APS_ASDU_TOO_LONG_STATUS = 0xa0,
/** A received fragmented frame can not be defragmented currently. */
APS_DEFRAG_DEFERRED_STATUS = 0xa1,
/** A received fragmented frame can not be defragmented, because the device
* does not support fragmentation. */
APS_DEFRAG_UNSUPPORTED_STATUS = 0xa2,
/** APS is in a state when request's execution is impossible. */
APS_ILLEGAL_REQUEST_STATUS = 0xa3,
/** An APSME-UNBIND.request has failed, because the requested binding link does not
* exist in the binding table. */
APS_INVALID_BINDING_STATUS = 0xa4,
/** An APSME-REMOVE-GROUP.request has been issued with a group identifier
* that is absent in the group table. */
APS_INVALID_GROUP_STATUS = 0xa5,
/** A parameter's value is invalid or out of range. */
APS_INVALID_PARAMETER_STATUS = 0xa6,
/** An APSDE-DATA.request requesting acknowledged transmission has failed
* because of no acknowledgement being received. */
APS_NO_ACK_STATUS = 0xa7,
/** An APSDE-DATA.request with the destination addressing mode set to 0x00
* has failed, because no devices are bound to this device. */
APS_NO_BOUND_DEVICE_STATUS = 0xa8,
/** An APSDE-DATA.request with the destination addressing mode
* set to 0x03 has failed, because the corresponding short address has not been found
* in the address map table. */
APS_NO_SHORT_ADDRESS_STATUS = 0xa9,
/** An APSDE-DATA.request with the destination addressing mode set to 0x00
* has failed, because the binding table is not supported on the device. */
APS_NOT_SUPPORTED_STATUS = 0xaa,
/** An ASDU secured using a link key has been received . */
APS_SECURED_LINK_KEY_STATUS = 0xab,
/** An ASDU secured using a network key has been received. */
APS_SECURED_NWK_KEY_STATUS = 0xac,
/** An APSDE-DATA.request requesting security has resulted in an error
* during the corresponding security processing. */
APS_SECURITY_FAIL_STATUS = 0xad,
/** An APSME-BIND.request or APSME.ADDGROUP.request have been issued ,while the binding
* table or the group table, respectively, is full. */
APS_TABLE_FULL_STATUS = 0xae,
/** An unsecured ASDU has been received. */
APS_UNSECURED_STATUS = 0xaf,
/** An APSME-GET.request or APSMESET.request has been issued with an
* unknown attribute's identifier. */
APS_UNSUPPORTED_ATTRIBUTE_STATUS = 0xb0,
/** An ASDU secured using the trust center link key has been received. */
APS_SECURED_TRUST_CENTER_LINK_KEY_STATUS = 0xb1,
/** An ASDU secured using the trust center's link key's hash has been received. */
APS_SECURED_HASH_OF_TRUST_CENTER_LINK_KEY_STATUS = 0xb2,
/** An invalid or out-of-range parameter has been passed to a primitive from
* the next higher layer. */
APS_NWK_INVALID_PARAMETERS_STATUS = 0xC1,
/** The next higher layer has issued a request that is invalid or cannot be
* executed given the current state of the NWK layer. */
APS_NWK_INVALID_REQUEST_STATUS = 0xC2,
/** An NLME-JOIN.request has been disallowed. */
APS_NWK_NOT_PERMITTED_STATUS = 0xC3,
/** An NLME-NETWORK-FORMATION.request has failed to start a network. */
APS_NWK_STARTUP_FAILURE_STATUS = 0xC4,
/** A device with the address supplied to the NLMEDIRECT-JOIN.request is
* already present in the neighbor table of the device on which
* the NLME-DIRECT-JOIN.request has been issued. */
APS_NWK_ALREADY_PRESENT_STATUS = 0xC5,
/** An NLME-SYNC.request has failed at the MAC layer. */
APS_NWK_SYNC_FAILURE_STATUS = 0xC6,
/** An NLME-JOIN-DIRECTLY.request has failed, because there the neighbor table is full. */
APS_NWK_NEIGHBOR_TABLE_FULL_STATUS = 0xC7,
/** An NLME-LEAVE.request has failed, because the device addressed in
* the parameter list is not in the neighbor table of the issuing device. */
APS_NWK_UNKNOWN_DEVICE_STATUS = 0xC8,
/** An NLME-GET.request or NLME-SET.request has been issued with
* an unknown attribute's identifier. */
APS_NWK_UNSUPPORTED_ATTRIBUTE_STATUS = 0xC9,
/** No networks has been detected after an NLME-JOIN.request has been issued. */
APS_NWK_NO_NETWORKS_STATUS = 0xCA,
/** Security processing has been attempted on an outgoing frame
* and has failed, because the frame counter has reached its maximum value. */
APS_NWK_MAX_FRM_COUNTER_STATUS = 0xCC,
/** Security processing has been attempted on an outgoing frame
* and has failed, because no key was available with which to process it. */
APS_NWK_NO_KEY_STATUS = 0xCD,
/** Security processing has been attempted on an outgoing frame
* and has failed, because the security engine produced erroneous output. */
APS_NWK_BAD_CCM_OUTPUT_STATUS = 0xCE,
/** An attempt to discover a route has failed because of a lack of routing table's
* or discovery table's capacity. */
APS_NWK_NO_ROUTING_CAPACITY_STATUS = 0xCF,
/** An attempt to discover a route has failed owing to a reason other
* than a lack of routing tables' capacity. */
APS_NWK_ROUTE_DISCOVERY_FAILED_STATUS = 0xD0,
/** An NLDE-DATA.request has failed due to a routing
* failure on the sending device. */
APS_NWK_ROUTE_ERROR_STATUS = 0xD1,
/** An attempt to send a broadcast frame or member mode multicast has failed,
* because there is no room in the broadcast transmission table. */
APS_NWK_BT_TABLE_FULL_STATUS = 0xD2,
/** An NLDE-DATA.request has failed owing to a lack of buffered space. */
APS_NWK_FRAME_NOT_BUFFERED_STATUS = 0xD3,
/** IEEE 802.15.4-2006, Table 78 MAC enumerations description. */
/** The frame counter purportedly applied by the originator of the
* received frame is invalid. */
APS_MAC_COUNTER_ERROR_STATUS = 0xDB,
/** The key purportedly applied by the originator of the received frame is
* not allowed to be used with that frame type according to the key usage
* policy of the recipient. */
APS_MAC_IMPROPER_KEY_TYPE_STATUS = 0xDC,
/** The security level purportedly applied by the originator of the received
* frame does not meet the minimum security level required/expected by
* the recipient for that frame type. */
APS_MAC_IMPROPER_SECURITY_LEVEL_STATUS = 0xDD,
/** The received frame was purportedly secured using security based on
* IEEE Std 802.15.4-2003, though such security is not supported by this standard.
**/
APS_MAC_UNSUPPORTED_LEGACY_STATUS = 0xDE,
/** The security purportedly applied by the originator of the received frame
* is not supported. */
APS_MAC_UNSUPPORTED_SECURITY_STATUS = 0xDF,
/** The beacon was lost following a synchronization request. */
APS_MAC_BEACON_LOSS_STATUS = 0xE0,
/** A transmission could not take place due to activity on the channel,
* i.e., the CSMA-CA mechanism has failed. */
APS_MAC_CHANNEL_ACCESS_FAILURE_STATUS = 0xE1,
/** The GTS request has been denied by the PAN coordinator. */
APS_MAC_DENIED_STATUS = 0xE2,
/** The attempt to disable the transceiver has failed. */
APS_MAC_DISABLE_TRX_FAILURE_STATUS = 0xE3,
/** Either a frame resulting from processing has a length that is
* greater than aMaxPHYPacketSize or a requested transaction is
* too large to fit in the CAP or GTS. */
APS_MAC_FRAME_TOO_LONG_STATUS = 0xE5,
/** The requested GTS transmission has failed because the specified
* GTS either does not have a transmit GTS direction or has not been defined. */
APS_MAC_INVALID_GTS_STATUS = 0xE6,
/** A request to purge an MSDU from the transaction queue was made using
* an MSDU handle that was not found in the transaction table. */
APS_MAC_INVALID_HANDLE_STATUS = 0xE7,
/** A parameter in the primitive is either not supported or is out of
* the valid range. */
APS_MAC_INVALID_PARAMETER_STATUS = 0xE8,
/** No acknowledgment was received after macMaxFrameRetries. */
APS_MAC_NO_ACK_STATUS = 0xE9,
/** A scan operation failed to find any network beacons. */
APS_MAC_NO_BEACON_STATUS = 0xEA,
/** No response data were available following a request. */
APS_MAC_NO_DATA_STATUS = 0xEB,
/** The operation failed because a 16-bit short address was not allocated. */
APS_MAC_NO_SHORT_ADDRESS_STATUS = 0xEC,
/** A receiver enable request was unsuccessful because it could not be
* completed within the CAP. */
APS_MAC_OUT_OF_CAP_STATUS = 0xED,
/** A PAN identifier conflict has been detected and communicated
* to the PAN coordinator. */
APS_MAC_PAN_ID_CONFLICT_STATUS = 0xEE,
/** A coordinator realignment command has been received. */
APS_MAC_REALIGNMENT_STATUS = 0xEF,
/** The transaction has expired and its information was discarded. */
APS_MAC_TRANSACTION_EXPIRED_STATUS = 0xF0,
/** There is no capacity to store the transaction. */
APS_MAC_TRANSACTION_OVERFLOW_STATUS = 0xF1,
/** The transceiver was in the transmitter enabled state when the receiver
* was requested to be enabled. */
APS_MAC_TX_ACTIVE_STATUS = 0xF2,
/** The key purportedly used by the originator of the received frame is
* not available or, if available, the originating device is not known
* or is blacklisted with that particular key. */
APS_MAC_UNAVAILABLE_KEY_STATUS = 0xF3,
/** A SET/GET request was issued with the identifier of a PIB
* attribute that is not supported. */
APS_MAC_UNSUPPORTED_ATTRIBUTE_STATUS = 0xF4,
/** A request to send data was unsuccessful because neither the source address
* parameters nor the destination address parameters were present. */
APS_MAC_INVALID_ADDRESS_STATUS = 0xF5,
/** A receiver enable request was unsuccessful because it specified a number
* of symbols that was longer than the beacon interval. */
APS_MAC_ON_TIME_TOO_LONG_STATUS = 0xF6,
/** A receiver enable request was unsuccessful because it could not be
* completed within the current superframe and was not permitted to be
* deferred until the next superframe. */
APS_MAC_PAST_TIME_STATUS = 0xF7,
/** The device was instructed to start sending beacons based on the
* timing of the beacon transmissions of its coordinator, but the device
* is not currently tracking the beacon of its coordinator. */
APS_MAC_TRACKING_OFF_STATUS = 0xF8,
/** An attempt to write to a MAC PIB attribute that is in a table failed
* because the specified table index was out of range. */
APS_MAC_INVALID_INDEX_STATUS = 0xF9,
/** There are some unscanned channels yet, but there is no memory */
APS_MAC_LIMIT_REACHED_STATUS = 0xFA,
/** A SET/GET request was issued with the identifier of an attribute
* that is read only. */
APS_MAC_READ_ONLY_STATUS = 0xFB,
/** A request to perform a scan operation failed because the MLME was
* in the process of performing a previously initiated scan operation. */
APS_MAC_SCAN_IN_PROGRESS_STATUS = 0xFC,
/** The device was instructed to start sending beacons based on the timing of
* the beacon transmissions of its coordinator, but the instructed start time
* overlapped the transmission time of the beacon of its coordinator. */
APS_MAC_SUPERFRAME_OVERLAP_STATUS = 0xFD
} APS_Status_t;
Description
APS status values used in most of standard primives.