3.6 Requests and Confirmations
In general, a function that performs an asynchronous request to a stack component has a
name ending with Req. The argument for such a function is a pointer to
a structure, the name of which comes from adding _t to the function’s
name, indicating a type. This reference manual refers to this structure as request
parameters. Its primary field is a pointer to a callback function, which the system
invokes to confirm the execution of the request. Besides the callback function, the
request parameters include a structure for confirmation parameters as a field. To derive
the name of this structure, the user can replace Req with
Conf in the original function’s name. For example, the
ZDO_StartNetworkReq function issues a network start request with
ZDO_StartNetworkReq (ZDO_StartNetworkReq_t *req), where ZDO_StartNetworkReq_t contains a confirm field of the
ZDO_StartNetworkConf_t type.
The user must declare an instance of the request parameters as a global variable because the confirmation callback’s argument specifically references the confirmation parameter’s field within the request parameters. This requires that the instance of request parameters exists after the invoking function loses control. In addition, the user must avoid reusing the instance while the current request remains in execution.
The status field within the confirmation parameters indicates the
success or failure of the request execution and, in the case of failure, provides the
reason. The system assigns the status from the values of an enumeration type defined for
each stack component, such as APS_Status_t. However, the value of the status field can exceed
the range defined by the enumeration, as failures can occur not only at the target layer
but also at lower layers during request execution.