3.2.1 USB Default Connection
The default connection between the PC and MPLAB ICD 5 unit is USB using a USB Type-C cable. It is recommended that you use the cable that comes with the kit to avoid communication issues.
Note: Only USB communications can be used for
trace.
Note: MPLAB Data Visualizer, whether as an
MPLAB X IDE included plugin or as a stand-alone application,
can only detect the debugger when it is using USB
communications.
If you have problems with the other types of communications, return to USB and then use the Manage Network Tools (MNT) dialog to switch to Ethernet again.