9.2.1 Memories to Program

Select the memories to be programmed into the target.

If “Erase All Before Program” is selected under Program Options, then all device memory will be erased before programming. To select only certain memories to program after erase, check the specific memory type. To preserve the value of memory of different types, check to preserve that memory type and check the specific memory type; checking “Preserve Memory” writes the current contents to a buffer before erase, and checking “Memory” writes the contents back into that memory after erase, where Memory is the type of memory, such as EEPROM.

Table 9-1. Memories to Program Option Category
Auto select memories and rangesAllow ICD 5 to Select Memories – The debugger uses your selected device and default settings to determine what to program.

Manually select memories and ranges – You select the type and range of memory to program (see below).

Configuration Memory (always programmed in debug mode)Check to program configuration memory in release mode. For dual partition devices, another selection for partition 2 will be available.
MemoryCheck to program Memory. Types of memory include: Instruction RAM, Flash Data, Data Flash, EEPROM, ID, Boot Flash, Auxiliary.
Memory Range(s) (hex)*The starting and ending hex address range in Memory. Types of memory include: Instruction RAM.
Program MemoryCheck to program the target program memory range specified below.
Program Memory Range(s) (hex)*The starting and ending hex address range in program memory for programming, reading, or verification.
Note: The address range does not apply to the Erase function. The Erase function will erase all data on the device.
Preserve Program MemoryCheck to not program the target program memory range specified below.

Ensure code is NOT code protected.

Preserve Program Memory Range(s) (hex)*The starting and ending hex address range in target program memory to preserve when programming, reading, or verifying.

This memory is read from the target and overlayed with existing MPLAB X IDE memory.

Preserve MemoryCheck to preserve Memory for reprogramming. Types of memory include: Instruction RAM, Flash Data, Data Flash, EEPROM, ID, Boot Flash, Auxiliary.

Ensure code is NOT code protected.

Preserve Memory Range(s) (hex)*The starting and ending hex address range in target Memory to preserve when programming, reading, or verifying. Types of memory include: Instruction RAM, Flash Data, Data Flash, EEPROM, Boot Flash, Auxiliary.

This memory is read from the target and overlayed with existing MPLAB X IDE memory.

Ensure code is NOT code protected.

* If you receive a programming error due to an incorrect range, ensure the range does not exceed available/remaining device memory.