1.11 DMAC usart echo
This example application demonstrates USART transfer with DMA to receive 10 bytes and echo back the received bytes
Description
This application demonstrates USART transfer with DMA using SERCOM peripheral configured in USART mode. One DMA channel is used to receive 10 bytes of data from the USART and another DMA channel is used to echo back the received bytes.
Downloading and building the application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/dmac/dmac_usart_echo/firmware .
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32mm_usb_curiosity.X | MPLABX project for PIC32MM USB Curiosity board |
Setting up the hardware
The following table shows the target hardware for the application projects.
| Project Name | Board |
|---|---|
| pic32mm_usb_curiosity.X | PIC32MM USB Curiosity board |
Setting up PIC32MM USB Curiosity board
To run the demo, the following additional hardware are required:
Connect micro USB cable to the 'USB1' on the board to the computer
Install an USB UART click board on to the mikroBUS socket J4
Connect mini USB cable between PC and the USB UART click board
Note: Ensure that the series resistors on the mikroBUS headers are of value 0 Ohms
Running the Application
Open the Terminal application (Ex.:Tera term) on the computer
Connect to the "USB to UART" COM port and configure the serial settings as follows:
Baud : 115200
Data : 8 Bits
Parity : None
Stop : 1 Bit
Flow Control : None
Build and Program the application project using its IDE
Following message is output on console:

Type 10 characters in the terminal. It will echo back the received bytes and toggles the LED
The following table provides the LED name:
| Board | LED Name |
|---|---|
| PIC32MM USB Curiosity board | LED1 |