1.3 CCP Compare Mode

This example shows how to use the CCP module in compare mode to generate an dual edge, active high, and toggle output on compare match.

Description

Three TC channels are configured in compare mode. Each channel generates different output waveform depending upon configured action on compare match and period match.

  • Dual Edge output: Output is set high on compare A match and is set low on compare B match.

  • Active high output: Output is set high on compare A match and remains high.

  • Toggle output: Output toggles on compare A match.

Downloading and building the application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/ccp/ccp_compare_mode/firmware .

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32mm_usb_curiosity.XMPLABX project for PIC32MM USB Curiosity board

Setting up the hardware

The following table shows the target hardware for the application projects.

Project NameBoard
pic32mm_usb_curiosity.XPIC32MM USB Curiosity board

Running the Application

  1. Build and program the application project using its IDE

  2. Observe generated waveforms on the oscilloscope

OC PinPort PinObservable characteristic of the waveform
OCM1ARA12 (Pin on J12)Dual Edge ouptut with 5 kHz frequency
OCM4RA7 (Pin on J12)Active high output
OCM2DRB1 (Pin on J4)Toggle output with 2.5 kHz frequency