1.18 SPI EEPROM write read

This example application demonstrates how to use the SPI peripheral to write and read from the SPI serial EEPROM memory.

Description

This example uses the SPI peripheral library to write an array of values to the SPI Serial EEPROM and verify the value written by reading the values back and comparing it to the value written. The example application performs the EEPROM writing only once after a power on reset.

Downloading and building the application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/spi/master/spi_eeprom_write_read/firmware .

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32mm_usb_curiosity.XMPLABX project for PIC32MM USB Curiosity board

Setting up the hardware

The following table shows the target hardware for the application projects.

Project NameBoard
pic32mm_usb_curiosity.XPIC32MM USB Curiosity board

Setting up PIC32MM USB Curiosity board

  • To run the application, following additional hardware are required:

  • Connect micro USB cable to the 'USB1' connector on the board to the computer

  • Plug the EEPROM 4 Click board into the MikroBus socket J4 of the development board

  • Note: Ensure that the series resistors on the mikroBUS headers are of value 0 Ohms

Running the Application

  • Build and program the application using its IDE

  • LED indicates the success or failure:

    • LED is turned ON when the value read from the EEPROM matched with the written value

    • LED is turned OFF when the value read from the EEPROM did not match with the written value

Following table provides LED names: