1.16 RCON reset handler
This example shows how to use the RCON peripheral to indicate the cause of the device reset and clear the reset causes.
Description
The Reset module combines all Reset sources and controls the device Host Reset signal, SYSRST. The Reset module allows the reset source to be identified and it clears the reset cause through software.
This example application uses the RCON peripheral to indicate the MCLR and the Watchdog reset. The WDT reset is emulated by not feeding the watchdog on switch press.
Downloading and building the application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/rcon/reset_handler/firmware .
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32mm_usb_curiosity.X | MPLABX project for PIC32MM USB Curiosity board |
Setting up the hardware
The following table shows the target hardware for the application projects.
| Project Name | Board |
|---|---|
| pic32mm_usb_curiosity.X | PIC32MM USB Curiosity board |
Setting up PIC32MM USB Curiosity board
To run the demo, the following additional hardware are required:
Connect micro USB cable to the 'USB1' connector on the board to the computer
Install an USB UART click board on to the mikroBUS socket J4
Connect mini USB cable between PC and the USB UART click board
Note: Ensure that the series resistors on the mikroBUS headers are of value 0 Ohms
Running the Application
Open the Terminal application (Ex.:Tera term) on the computer
Connect to the "USB to UART" COM port and configure the serial settings as follows:
Baud : 115200
Data : 8 Bits
Parity : None
Stop : 1 Bit
Flow Control : None
Build and Program the application project using its IDE
Following message is output on console:

Watch dog timer is fed periodically using Core Timer to prevent the WDT reset and the LED is toggled
Following table provides the switch and the LED name:
Board LED Name Switch Name PIC32MM USB Curiosity board LED1 S3 Press the switch to put the system in deadlock
LED should stop blinking and the console should print the following message

The WDT will reset the device in four seconds and the demonstration should restart