8.2 Defining And Using Bits
The interrupt routine shown in this chapter modifies a flag that is used by main-line code to set the state of the LED. The flag's state is set by the ISR. As this flag only needs to hold a true or false value, it was defined as a bit object to save on storage space and make checking its contents more efficient.
bit psect flag with the psect that holds them. The only difference
to the following code extract compared to the that for the Mid-range device is that the
psect was placed in the Access
bank.PSECT bitbssCOMMON,bit,class=COMRAM,space=1
LEDState:
DS 1 ;a single bit used to hold the required LED stateBit symbols are used in PIC18 code in the same way as for Mid-range devices. The file
register address of a bit symbol can be obtained by dividing the bit address by 8, and
the bit position can be obtained by taking the bitwise AND with 7. And as with Mid-range
devices, once you include <xc.inc> into your program, bit symbols
are defined for bits within special function registers, such as TMR0IF
and GIEH, which were used in the example code.
bsf IPEN, but rather, the operand
to this instruction was specified as the INTCON0 file register address and a special
symbol used to locate the IPEN bit within this
register.PSECT code
start:
bsf BANKMASK(INTCON0),INTCON0_IPEN_POSN,c ;set IPEN bit In this particular case, attempting to use the IPEN bit directly would result in an
undefined symbol error. This is because the 18F47K42 device has more than one bit within
its SFRs called IPEN. The other is the IPEN bit in the ADCON1 register. In such
instances, the name IPEN is not unique and no bit symbol will be available in the
provided headers. You must access the bit using the SFR name, but the headers do provide
macros that represent the bit position, such as the INTCON0_IPEN_POSN,
used above. The same headers also supply macros which indicate the number of bits in the
SFR, e.g., _INTCON0_IPEN_SIZE and a mask you can use for bitwise logic
operations, e.g., _INTCON0_IPEN_MASK. These macros are available for
every SFR bit, and you can use them in preference to the bit name if you prefer.