8.3 Building the Example
timedLED.S, for example, it could be built using the command below.
Note that the file name uses an upper case .S extension so that the
file is preprocessed before any other
processing.pic-as -mcpu=18F47K42 -Wl,-presetVec=0h -Wl,-pivt=08h -Wa,-a -Wl,-Map=timedLED.map timedLED.SThe ivt psect holding the vector table was linked to address 0x8. The
link address of this psect is used in the source code to load the value contained in the
IVTBASE register, to ensure that the device reads the correct vectors when an interrupt
occurs. The address you specify for this psect must be a multiple of two to ensure the
requirement imposed by the reloc flag used with this psect is met. If
you were to attempt to link the psect at an odd address, an error will be issued.
The above command also includes the -Wl,-Map=timedLED.map option to
generate a map file and the -Wa,-a option to generate an assembly list
file, which will be called timedLED.lst.
If you are building in the MPLAB X IDE, add additional linker
options (such as those specified using the driver option
-Wl,linkerOption) to the Custom
linker options field in the category in the Project Properties dialog. When adding options to this
field, do not include the leading -Wl,, as this prefix is added in by
the IDE. Specify additional options to the assembler (such as the
-Wa,assemblerOption) in the
Additional options field in the pic-as Global
Options category (the leading -Wa, must be specified).
See Building the Example for screen
captures showing where these additional options should be added.