3 A Basic Example For PIC18 Devices
As an introduction to the PIC Assembler, consider the following example of a complete assembly program. It is written for a PIC18F47K42 device, but much of this example is also applicable for other devices. The code performs the mundane task of repeatedly reading the value on PORTA and recording the highest value that has been read. Aspects of this program are discussed in the sections that follow.
Note: This code example performs manual masking of instruction
operand addresses to avoid fixup overflow errors. You can alternatively have the
linker automatically truncate operand values when building, as discussed in Working with Data Banks, so that the
BANKMASK() and PAGEMASK() macros used in this
example are not required.A Basic PIC18 Example
/* Find the highest PORTA value read, storing this into
the object max */
PROCESSOR 18F47K42
#include <xc.inc>
CONFIG "FEXTOSC = OFF" // Ext Oscillator Selection->Oscillator not enabled
CONFIG "RSTOSC = HFINTOSC_1MHZ" // Reset Osc Select->HFINTOSC,HFFRQ=4MHz,CDIV=4:1
CONFIG "CLKOUTEN = OFF" // Clock out Enable bit->CLKOUT function is disabled
CONFIG "PR1WAY = ON" // PRLOCKED 1-Way Set->PRLOCK cleared/set only once
CONFIG "CSWEN = ON" // Clock Switch Enable->Writing to NOSC & NDIV allowed
CONFIG "FCMEN = ON" // Fail-Safe Clock Monitor->Clock Monitor enabled
CONFIG "MCLRE = EXTMCLR" // If LVP=0, MCLR pin is MCLR; LVP=1, RE3 pin is MCLR
CONFIG "PWRTS = PWRT_OFF" // PWRT is disabled
CONFIG "MVECEN = OFF" // Vector table isn't used to prioritize interrupts
CONFIG "IVT1WAY = ON" // IVTLOCK bit can be cleared and set only once
CONFIG "LPBOREN = OFF" // ULPBOR disabled
CONFIG "BOREN = SBORDIS" // Brown-out Reset enabled, SBOREN bit is ignored
CONFIG "BORV = VBOR_2P45" // Brown-out Reset Voltage (VBOR) set to 2.45V
CONFIG "ZCD = OFF" // ZCD disabled, enable by setting ZCDSEN in ZCDCON
CONFIG "PPS1WAY = ON" // PPS locked after clear/set cycle
CONFIG "STVREN = ON" // Stack full/underflow will cause Reset
CONFIG "DEBUG = OFF" // Background debugger disabled
CONFIG "XINST = OFF" // Extended Instruction Set disabled
CONFIG "WDTCPS = WDTCPS_31" // Divider ratio 1:65536; software control of WDTPS
CONFIG "WDTE = OFF" // WDT Disabled; SWDTEN is ignored
CONFIG "WDTCWS = WDTCWS_7" // window open 100%; software control
CONFIG "WDTCCS = SC" // Software Control
CONFIG "BBSIZE = BBSIZE_512" // Boot Block size is 512 words
CONFIG "BBEN = OFF" // Boot block disabled
CONFIG "SAFEN = OFF" // SAF disabled
CONFIG "WRTAPP = OFF" // Application Block not write protected
CONFIG "WRTB = OFF" // Configuration registers not write-protected
CONFIG "WRTC = OFF" // Boot Block (000000-0007FFh) not write-protected
CONFIG "WRTD = OFF" // Data EEPROM not write-protected
CONFIG "WRTSAF = OFF" // SAF not Write Protected
CONFIG "LVP = ON" // LV programming enabled, MCLR pin, MCLRE ignored
CONFIG "CP = OFF" // PFM and Data EEPROM code protection disabled
GLOBAL max ;make this global so it is watchable when debugging
;objects in common (Access bank) memory
PSECT udata_acs
max:
DS 1 ;reserve 1 byte for max
tmp:
DS 1 ;1 byte for tmp
;this must be linked to the reset vector
PSECT resetVec,class=CODE,reloc=2
resetVec:
goto main
/* find the highest PORTA value read, storing this into
the object max */
PSECT code
main:
;set up the oscillator
movlw 0x62
movlb 57
movwf BANKMASK(OSCCON1),b
movlw 2
movwf BANKMASK(OSCFRQ),b
movlb 58
clrf BANKMASK(ANSELA),b ;select digital input for port A
clrf max,c ;starting point
loop:
movff PORTA,tmp ;read and store the port value
movf tmp,w,c ;is this value larger than max?
subwf max,w,c
bc loop ;no - read again
movff tmp,max ;yes - record this new high value
goto loop ;read again
END resetVec