5.1 Multiple Source Files and Shared Access
Your assembly program can be split into as many source files as required. Doing so will make the source code easier to manage and navigate, but there are steps you must take to share objects and routines between modules, and your code will need to take into account where routines in other modules might ultimately be located.
To access an object or routine define in another source file, there are two steps that
need to be followed. First, when you define the object or routine, you must tell the
linker to allow the symbol (label) to be globally accessible. This is done using the
GLOBAL directive. Next, you must declare the same symbol in every
other file that needs to access it to inform the linker that this symbol is linked to a
definition in another module. This can be done using either the GLOBAL
or EXTRN directive.
file_1.S contains the
definition for the object count, which is essentially a label
associated with reserved storage space, as shown
below.GLOBAL count
PSECT udata_shr
count:
DS 1 ;1 byte in common memoryAs count must be accessible from other modules, a GLOBAL
count directive was used in addition to the symbol's definition, as shown
above, to tell the linker that declarations of the same symbol in other modules can link
to the definition in this module.
In file_2.S, another GLOBAL count directive was used to
declare the symbol and link this with the definition of count that the
linker will ultimately find in the file_1.o module. You may prefer to
use the EXTRN count directive to perform this function. This directive
performs a similar task to GLOBAL, but it will trigger an error if the
directive appears in the same module that contains the symbol's definition.
The same mechanism is used for symbols used by routines that need to be accessible from
more than one module. In this example, the code in file_2.S contains a
GLOBAL storeLevel directive to allow the symbol to be referenced
from outside that module, and file_1.S contains the same directive to
link the storelevel symbol in that module with its definition in the
other. Again, an EXTRN storeLevel directive could have been used in
file_1.S to ensure the symbol is defined in the module you
expect.