5.3 Linear Memory
The linear addressing mode is a means of accessing the banked data memory on Enhanced Mid-range devices as one contiguous and linear block. Your device data sheet will indicate if this memory is implemented on your device and contain further operational details.
Linear memory is typically used for objects that are too large to fit into a single memory bank, but it is important to remember that linear memory is not present in addition to a device's regular banked memory; it is simply an alternate way to access that banked memory. You have to define objects larger than a bank in a different way to ordinary objects that are placed into banked memory.
DLABS directive, shown
here.;define NUM_TO_READ bytes of linear memory, at banked address 0x120
DLABS 1,0x120,NUM_TO_READ,levelsThis directive takes several arguments. The first is the address space in which the memory will be defined. This should be the value 1 for objects to be placed in data memory. The second argument is the starting address for the storage. This can be specified as either a linear or banked address. The equivalent linear address for the banked address 0x120, as used above, is 0x20A0, for example. The following argument is the number of bytes that is to be reserved. In this case, a preprocessor macro has been used to represent the array size. This macro has been defined in the build options, as shown in section Building the Example. The final argument is a symbol. This is optional and creates a label for the object at the indicated address.
Unlike most directives, the DLABS directive does not produce output that
is part of the current psect, so it can appear at any location in the source file. This
also means that there should not be a label placed immediately before the directive. If
a label is required for the object you are defining, then specify it as the last
argument of the directive, as shown above.
levels object
in banks 2 and 3, as specified by the address used with the directive. While it is
possible to access this memory using the ordinary file register instructions, such
access can become problematic if the offset into the array is not known, as it is not
clear which bank needs to be selected beforehand. The Enhanced Mid-range devices,
however, allow you to use the FSR register to indirectly read and write data memory
using a linear address and without banking. Accessing levels indirectly
is shown in the example and is repeated
here.storeLevel:
movwf tmp ;store the parameter
movf count,w ;add the count index to...
addlw low(levels) ;the linear base address of the array...
movwf FSR1L ;storing the result in FSR1
movlw high(levels)
clrf FSR1H
addwfc FSR1H
movf tmp,w ;retrieve the parameter
movwf INDF1 ;access levels using linear memorySince it was defined using the DLABS directive, the symbol
levels will always represent a linear address. This is still true
even if a banked address was used as the second argument to this directive. Such an
address can be loaded directly into an FSR register when linear access is required. The
linear address value of the symbol can be found in the assembly list file and also in
the map file if the symbol was made globally accessible using the
GLOBAL directive.