7.4 Building the Example
timedLED.S, for example, it could be built using the command below.
Note that the file name uses an upper case .S extension so that the
file is preprocessed before any other
processing.pic-as -mcpu=16F18446 -Wl,-presetVec=0h -Wl,-pisrVec=04h -Wa,-a -Wl,-Map=timedLED.map timedLED.SThe psect containing the reset code has been linked to address 0 and in addition, the
psect holding the interrupt routine was linked to the device's vector location, address
0x4. The command also includes the -Wl,-Map=timedLED.map option to
generate a map file and the -Wa,-a option to generate an assembly list
file, which will be called timedLED.lst.
If you are building in the MPLAB X IDE, add additional linker
options (such as those specified using the driver option
-Wl,linkerOption) to the Custom
linker options field in the category in the Project Properties dialog. When adding options to this
field, do not include the leading -Wl,, as this prefix is added in by
the IDE. Specify additional options to the assembler (such as the
-Wa,assemblerOption) in the
Additional options field in the pic-as Global
Options category (the leading -Wa, must be specified).
See Building the Example for screen
captures showing where these additional options should be added.