4.1 Assembler Macros
An assembler macro was defined and used in this chapter's example program.
Assembler macros perform a similar function to the preprocessor's
#define directive, in that they define a single identifier to
represent a sequence of code. When a large amount of code spread over multiple lines is
to be represented, assembler macro definitions might be easier to read than preprocessor
macros.
skipnc MACRO
btfsc CARRY
ENDMThis creates a macro that skips the following instruction based on the carry bit in the STATUS register. Bit access of SFRs is described later, in section Defining And Using Bits.
subwf max^(tmp&0ff80h),w
skipnc
goto loopAn assembler macro can have arguments, too, and there are several characters that have special meaning inside macro definitions. A full description of these are presented in the MPLAB® XC8 PIC Assembler User's Guide.