11.3.2 Interrupt Vector Table Contents
MVECEN = 0
When MVECEN = 0, the address location pointed to by IVTBASE has a
GOTO instruction for a high-priority interrupt. Similarly, the corresponding
low-priority vector also has a GOTO instruction, which is executed in case of a
low-priority interrupt.
MVECEN = 1
When MVECEN = 1, the value in the vector table of each interrupt points to the
address location of the first instruction of the Interrupt Service Routine, hence: ISR Location =
Interrupt Vector Table entry << 2.