10.3.10.6 Reading the Program Flash Memory
The TBLRD instruction retrieves data from program
memory at the location to which the TBLPTR register points and places it into the TABLAT SFR register. Table reads from program memory are performed one byte at a
time. The instruction set includes incrementing the TBLPTR register automatically for the
next table read operation.
The CPU operation is suspended during the read and resumes operation immediately after. From the user point of view, the value in the TABLAT register is valid in the next instruction cycle.
The internal program memory is typically organized by words. The Least Significant bit of the address selects between the high and low bytes of the word. The following figure illustrates the interface between the internal program memory and the TABLAT register.
Reading a Program Flash Memory Word
MOVLW CODE_ADDR_UPPER ; Load TBLPTR with the base MOVWF TBLPTRU ; address of the word MOVLW CODE_ADDR_HIGH MOVWF TBLPTRH MOVLW CODE_ADDR_LOW MOVWF TBLPTRL READ_WORD: TBLRD*+ ; read into TABLAT and increment MOVF TABLAT, W ; get data MOVWF WORD_EVEN TBLRD*+ ; read into TABLAT and increment MOVFW TABLAT, W ; get data MOVF WORD_ODD