10.3.10.5 Table Pointer Boundaries
The TBLPTR register is used in reads of the Program Flash Memory. Writes using the TBLPTR register go into a buffer RAM from which the data can eventually be transferred to Program Flash Memory using the NVMADR register and NVM commands.
When a TBLRD instruction is
executed, all 22 bits of the TBLPTR determine which byte is read from program memory
directly into the TABLAT register.
When a TBLWT instruction is
executed, the byte in the TABLAT register is written not to Flash memory but to a buffer
register in preparation for a program memory write. All the buffer registers form a write
block of size 128 words/256 bytes. The LSbs of the TBLPTR register determine to which
specific address within the buffer register block the write affects. The size of the write
block determines the number of LSbs that are affected. The MSbs of the TBLPTR register have
no effect during TBLWT operations.
When a program memory page write is executed, the entire buffer register block is written to the Flash memory at the address determined by the MSbs of the NVMADR register. The LSbs are ignored during Flash memory writes.
The following figure illustrates the relevant boundaries of the TBLPTR register based on NVM operations.
- Refer to the “Memory Organization” chapter for more details about the size of the buffer registers block.