23.2.1 POR and Voltage Monitors
To prevent improper operation of the level shifters at low voltage, a Power-on Reset (POR) circuit is included. The POR circuit is automatically enabled on supply power up and holds the corresponding voltage domain logic in reset state until the power supply has reached sufficient voltage for the corresponding voltage domain logic to operate properly. Once this supply voltage is reached, the POR circuit on that voltage domain will power itself down to save power, and re-arm itself if the supply voltage drops too low. For VDD power domain, the device’s main POR circuit is used whereas for VDDIOx domain, a separate POR circuit is included in the MVIO domain. The POR and PORVDDIOx bits in the PCON0 and PCON1 registers are used to represent when the corresponding voltage domain has recovered from a POR reset.
- The first voltage monitor is powered using the main VDD supply and becomes active when VDD reaches a sufficient voltage level. This voltage monitor is used to monitor the VDDIOx voltage level threshold has been achieved for level shifters to work.
- The second voltage monitor is powered using the VDDIOx supply and becomes active when VDDIOx reaches a sufficient voltage level. This voltage monitor is used to monitor the main VDD voltage level threshold has been achieved for level shifters to work.
This cross-coupled approach to voltage monitoring ensures that both – the monitor’s current domain and the opposite voltage domain have reached the sufficient voltage for level shifters to operate safely. Refer to Figure 23-1 for clarification. Refer to the Power Sequencing section for different ways to power up both the voltage domains.