45.5.2 Crystal Oscillator
The following figure illustrates a typical example of the crystal oscillator schematic:
The crystal must be located as close as possible to the device. Long signal lines may cause a load too high to operate the crystal, and cause crosstalk to other parts of the system.
| Signal Name | Recommended Pin Connection | Description |
|---|---|---|
| XIN | Load capacitor CLEXT(1)(2) | External crystal between 0.4 to 32 MHz |
| XOUT | Load capacitor CLEXT(1)(2) |
- Use the equation in Crystal Oscillator Characteristics to calculate CLEXT.
- Decoupling capacitor should be placed close to the device for each supply pin pair in the signal group.